This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMC555 astable frequency question

Other Parts Discussed in Thread: LMC555

the formula in LMC555 astable condition is not matching. I put the parameters as figure2 of LMC555 datasheet, the maximum frequency is around 9MHz and not matching to datasheet describe(3Mhz maximum in astable mode). Is there anything i miss?

  • Hi Peter,

    Formula 4 in the datasheet works best in the range as shown in Figure 8 of the datasheet.  As the operation is placed into the higher frequencies that are not shown in the graph it gets inaccurate.  This is caused by the LMC555 itself, along with the parasitics in the circuit.  In the higher frequencies the formula will need to be used as a staring point and then the parts adjusted to get the performance needed.


    Mike