Using the CDCLVC1108 to drive 8 output clocks to similar devices. F = 40 MHz. VDD = 3.3V, but receiving devices require clock signal between 1VPP and 2VPP. Trace length is about 100mm (50 ohm). Looking for a low power method to terminate CDCLC1108 outputs.
A simple 50 ohm parallel termination or a Thevenin termination with 100 ohm resistors would reduce the signal level well enough, and this could be AC coupled into the receiving device. But with 8 clocks, thats seems like a lot of current for the driver to be sourcing/sinking.
However, are there lower power alternatives? For example, could one use a series termination at the driver and then use a higher resistance voltage divider at the far end of the trace to attenuate the signal? If so, would it matter which side of the AC coupling cap the divider sits on? These are point-to-point connections for each driver output.