Hi All,
I use CD4013BE for my design and I am having these questions, please help:
I use only half of the CD4013BE:
Pin 1: Q
Pin 2: Q_bar
Pin 7 and Pin 14: GND and VDD +12VDC respectively
Pin 3: Clock
Pin 5: Data
Pin 4, Pin 6: Tied to GND
Should the IC's all other pins be tied to GND too? The problem I have is intermittent. I sometimes see the Output of Q and Q_bar on at the same time but they are not supposed to be. Is that could be my timing between the CLK and DATA or no?
Thank you