Hello!
I put one of these parts on a test board as a clock generator to free up the arb gen on the bench. I have a 25MHz xtal and would need 25, 4, and 3 MHz and maybe others. I was trying to figure out the I2C write sequence to make that happen but there is unfortunately no basic programming example in the datasheet, just reference to the demo software. I have the part live on my board, so I'm past the EVM demo stage.
There seems to be missing information regarding the setting of the registers. On page 19, Table 12, there is reference to: "... for more information, see the PLL Multiplier/Divider Definition paragraph..." which doesn't appear anywhere. Does anyone have a register write sequence to make simple clock frequency changes?
Thanks!
i.