This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Harmonic level become very high after lmk00101

Other Parts Discussed in Thread: LMK00101

Hi Bro,

I find a harmonic problem when using a lmk00101 output as reference source for a VCO (Analog/Hittile's HMC830)  then i test the lmk00101 separately.

I use a ocxo(10MHz/5x10(-8)ppm/clipped sine-wave/amplitude 0dBm@10MHz,-50dBm@20MHz,-60dBm@30MHz) connect to lmk00101's CLKin and measure its output leve. After LMK00101 we got a result: +8dBm@10MHz, -28dBm@20MHz,-2dBm@30MHz and the level reach -50dBm@3GHz even at 5GHz band we could see many signals in spectrum analyzer. When add an adjustable attenuator at OCXO output but it make no effect and lmk00101 lost its output at attenuate value reach 20dB.

I guess the lmk00101 do not work properly could many one give me some advice to solve this problem  ?

Thanks a lot.

Roger