Hi,
I would like to use TPL5010 as wake up timer and watchdog timer.
Hence, I'm going to connect TPL5010's RSTn output to CPU's reset, and WAKE, DONE signal to CPU's GPIOs.
My question is related to TPL5010's RSTn output:
For the first time of board powering, while the CPU is not programed yet, does TPL5010's RSTn output will be asserted following any timeout ?
I've read in the forum that: " The TPL will not output a WAKE if no DONE input is received. Instead, a periodic RSTn signal will take place. " and my concern is how should I program/flash the CPU while TPL5010 assert RSTn signal periodically ?
Thanks,
Shuli
RSTn