Other Parts Discussed in Thread: CDCE72010
Hello,
I got two questions on cdce72010 and its EVM:
1). I tried to use Webench designer to figure out my frequency design, but failed to get meaningful results. So I wonder if there is a solution for my design using cdce72010 EVM :
My input reference is at 100 MHz, VCXO is default at 491.52MHz, output needs 12.5MHz, although anything between 12 - 13 MHz also acceptable.
2). One additional question is for M, N dividers - are these dividers can handle divide-by odd-number such as the default divide-by-125 ? Also they can divide in step of 1, from 1 to 16384 ?
Thank you !
Du