Hello,
Originally I was typing this out on the Medical Hi-Rel forum because it involves the ADS52J90 but the more I typed, the more I realized this might be a question for you guys so here goes, let me know if it needs to be moved..
I have a customer who would like to check the compatibility of the JESD204b output from the ADS52J90 with their system.
The default scripts that come with this EVM only configure the LMK04286 device as simply a clock distribution device and relies on the user to provide an external clock via the SMA. So the onboard oscillators are not used.
The customer is running the JESD204b stream at 3.0Gbs and they need to provide the ADS52J90 with a 3Gbs/40 = 75MHz clock. So they're looking to generate that 75MHz clock using the onboard 100MHz clock oscillator paired with the LMK device. Is there anyway you could provide the required register settings to be able to do this?
He intends to edit the .cfg file that comes with the EVM, just to use that GUI. So he mostly needs the hex file register settings so he can manually edit the appropriate .cfg file (two hex files, one that outputs 75MHz and another which outputs 50MHz).
Please let me know if you nee dmore information or if there is something I am missing?
-Amanda