Hi E2E,
My customer is looking to get a 192MHz clock with low phase noise at 1kHz and 10kHz. The datasheet says integer mode will improve phase noise over non-integer mode but the Webench simulations show no difference. The sim reports -133.8dBc/Hz but the customer would like to see better performance. The datasheet suggests that it can do better than -133.8dBc/Hz. The customer is using the 'auto' loop-filter for both.
1. Should the customer switch to integer mode?
2. What sort of improvement can we expect from this change?
3. Is there any way to get the performance up?
Thanks,
-Sam