Part Number: CDCE913
I'm trying to use CDCE913 in +/- 150ppm range with 27MHz OSC to 27MHz LVCMOS 3.3V. but I can only adjust the frequency about +/-50ppm in my board.
(I used DSX321SH(27MHz/10pF/10ppm as XO source, the spec meets the requirement)
I think Changing the CL onchip can get +/- 150ppm, but I don't think this usage is correct?
In the datasheet, it's saying the pulling range is "min +/-120ppm, Nom. +/-150ppm."
Is there any limitation?
Also I checked document scaa085a.pdf. can anyone explain what Figure 4 and 6. mean?
I'm confused about them.
FIgure 4 is saying the pulling range is adjustable just by VCTRL.
Figure 6 is saying it's need to use CLonchip
Any advice or information you could provide would be greatly appreciated.