This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCLVC1104: Can the CDCLVC1104 pass DC signals?

Part Number: CDCLVC1104

Hi Team,

Can the CDCLVC1104 pass DC signals?  I see that the output frequency is listed with a minimum of DC.

Best Regards,
Brian Gosselin

  • Hi Brian,

    Yes.  DC input is lower than input thershold Vth of Vdd/2, then output will be logic low.  If the DC input is above Vth, then the output will be logic high.

    Regards,
    Alan