Other Parts Discussed in Thread: CODELOADER,
The outputs from two of this PLL won't aligned, in our case,
1. the clock to these two PLL are algined (in SYNC)
2. the SYNC signals to both PLL are aligned (in SYNC)
3. SYNC are enabled on all outputs of them
4. DDLY at their default
5. both PLL mode x"6"
Expect to see all outputs are aligned after toggling the SYNC as stated in the datasheet. Thanks.