I am using TICS Pro 1.4
I input 491.52MHz to the eval board and I am getting /16 of the VCO (431.25MHz) though according to the settings it should be /12 i.e 575MHz . I attached the settings as exported from TICS PRO. Any ideas of what is wrong?
Thanks
R64 0x4000AF R62 0x3E0000 R61 0x3D0001 R59 0x3B0000 R48 0x3003FC R47 0x2F00CF R46 0x2E0F23 R45 0x2D0075 R44 0x2C0000 R43 0x2B0000 R42 0x2A0000 R41 0x290800 R40 0x280000 R39 0x278204 R38 0x26002A R37 0x254000 R36 0x240820 R35 0x23099B R34 0x22C3F0 R33 0x214210 R32 0x204210 R31 0x1F0401 R30 0x1E0034 R29 0x1D0084 R28 0x1C2924 R25 0x190000 R24 0x180509 R23 0x178842 R22 0x162300 R20 0x14012C R19 0x130965 R14 0x0E018C R13 0x0D4000 R12 0x0C7003 R11 0x0B0018 R10 0x0A10D8 R9 0x090302 R8 0x081084 R7 0x0728B2 R4 0x041943 R2 0x020500 R1 0x01080A R0 0x00231C