This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03318: VIM limits

Part Number: LMK03318

Hi folks - 

Looking at the datasheet for LMK03318, on the 3-level inputs (REFSEL, GPIO[3:1]) I see only a TYP for VIM.  Do we have some guidance for how much variation to expect above and below the 0.9V TYP? 

For example, VIL is 0.4V, so is 0.6V going to be VIM? 0.7V? 

I assume there is some band which is indeterminate. 

Thanks much, 

Jake