Part Number: LMK61E2
Hi,
a) I would like to know how much time does it takes to change frequency:
1) Settling Time for Small Frequency Change
2) Settling Time for Large Frequency Change
b) Is there an EOL date for this IC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK61E2
Hi,
a) I would like to know how much time does it takes to change frequency:
1) Settling Time for Small Frequency Change
2) Settling Time for Large Frequency Change
b) Is there an EOL date for this IC?
Hi Haim,
The settling time for a frequency change will depend on what setting of the PLL you are changing to change the output frequency and by how much you are changing it. For example, changing the PLL N divider by 1 requires about 4us for the output frequency to settle (as the PLL must re-lock), while changing the output divider by 1 is faster and only requires about 2us for the output frequency to settle.
Is there a specific PLL control that you are changing that you need the settling time for? Or, you can provide me the initial frequency and the new frequency you wish to change to and I can test the specific case for you.
There is currently no EOL date for this device.
Regards,
-Tim
Hi Tim,
I would like to know what would be the maximum time (when making the largest possible change)?
Is there a formula that I can calculate it my self?
I would like to change the frequency with resolution of 5MHz, for example:
1) From 50MHz to 55MHz.
2) From 50MHz to 455MHz
3) From 55MHz to 695MHz