Part Number: LMK04828
Hi!
I have a custom board with LMK04828 in dual loop mode, it works fine until it comes to managing erroneous conditions on reference clock input (CLKin_0 in my case). I need the device to enter holdover (either fixed MAN_DAC or last tracked "good" point, doesn't matter now) both on "no signal on reference input" and on "reference frequency out of VCXO tuning range for PLL1 lock". I'm able to enter holdover only in conditions when:
1) HOLDOVER_EN & HOLDOVER_PLL1_DET are set and NO other holdover conditions are enabled;
2) MAN_DAC_EN and/or TRACK_EN are set;
3) reference signal lost from locked condition (i.e. when it was in range prior to being switched off).
The device DOES NOT enter holdover when reference clock goes too much low/high on frequency and PLL1 looses lock and when reference switching off in these conditions.
I have tried different modes with no success. If HOLDOVER_VTUNE_DET is enabled, the device does not enter holdover in any conditions, with different DAC trip settings and so on. Moreover, when VTUNE_DET is disabled, the device outputs DAC trip conditions correctly through CLKin_SEL0 pin, but if i turn VTUNE_DET ON, it stops doing so.
So, the main question is: how should i set up holdover settings for LMK04828 to enter holdover when the reference signal frequency goes out of range?
Thanks in advance,
Sergey