Part Number: TPL5111
tpl5111 in one shot mode, is there going to be a problem if Done pin should be left floating?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPL5111
tpl5111 in one shot mode, is there going to be a problem if Done pin should be left floating?
Hi Neo,
In any mode, if the DONE pin is not used, it should be grounded so there is no chance that noise or interference will cause the device to register a pulse.
Also, any method that drives the digital input pins to a logic high state can be used to control them. See Table 6.5: Electrical Characteristics.
Regards,
-Tim