Hello. Can someone send me the updated schematics for this board? I am having problems with this demoboard locking to the correct frequency. I am not sure if its the software or hardware. I can see that the internal vco oscillates and the reference oscillator is active but the GUI does not produce the desired frequency.
FYI I noticed that the schematics don't match the boards when I was looking for the CP filter. According to the schematics in the User guide, C1 and C2 should be part of the filter. However on the board, C1 and C2 are bypass caps for the VCC input.
The card that I am using has a date of 3/15/2016 and the online userguide is dated 2015.
Please assist.
Thnak you.