Part Number: LMK04828
Other Parts Discussed in Thread: TICSPRO-SW
Hi,
I've couple of questions regarding LMK04828 SYSREF generation.
1) I'm trying to generate continuous mode of SYSREF signal using LMK04828. When I probe my SYSREF signal, it always stays at logic HIGH (1.0V).
VCO frequency = 3000 MHz
SYSREF Clock Divider = 300
So I can generate SYSREF at 10 MHz continuously. I've configured my registers accordingly. Please check my register settings in the attached MAC file (codeloader4 settings). If you could provide me sample code or register flow to generate SYSREF - continuous mode, that would be really helpful.
2) After the registers are programmed from 0x000 to 0x1FFF, I'm not able to perform write event to any register.
For instance: if I want to write into Reg 0x143 once the programming sequence is done (0x000 - 0x1FFF), I am not able to perform write event. However I can read the old value back. Is it expected behavior?
Registers 0x1FFD - 0x1FFF are programmed to default values meaning that "Registers unlocked".
Please help me with the above inquiries.
Thanks,
Rekha