Part Number: LMX2531
To program the LMX2531LQ1778E in an Evaluation Board (ADC12D1x00RFRB), I used the following values in corresponding 24 bit registers as per the specifications of
foscin=60 MHz
fFout= 1800 MHz
R=8
N=240
(vco divider is disabled,delta-sigma modulator order=3,loop filter=2nd order)
But still I am not getting the output frequency at the output pin of LMX2531(pin no:21)
REG0 = 24'hF000_00
REG1 = 24'h2000_01
REG2 = 24'h4004_82
REG3 = 24'h7C80_03
REG4 = 24'h0000_04,
REG5 = 24'h8400_05, (INIT 1)
REG5 = 24'h8007_F5, (INIT 2)
REG6 = 24'h4866_56,
REG7 = 24'h05CB_07,
REG8 = 24'h0280_18,
REG9 = 24'h000B_A9,
REG12 = 24'h0104_8C
What is possible solutions?? please help..