Hi,
We want to interface LMK01801 with AD9783 - from Analog Devices.
Input clock frequency is roughly 1.32G and the output frequency from LMK01801 - 94.2 MHz going to AD9783.
Now my question is AD9783 has an input side termination of 50 ohm pulled upto common voltage of 400mV and Differential Peak-to-Peak Voltage (CLKP − CLKN) = maximum of 1.6V.
Now my doubt is at given common mode voltage of AD9873, what will be the maximum value of Vod generated from LMK01801 i.e. the output differential voltage. Whether it can cross the limits of AD9783? Or whether there is a problem in my understanding?
I will be thankful if I get quick help on this.
Regards.