This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCEL913: cdcel913

Part Number: CDCEL913

Hello,

I am using CDCEL913 to generate one 24MHz clock from output Y1,the  input refclk is 25MHz crystal,PLL1 is used. And I use I2C to register the chip.

But the ouput is not right ,and the Fvco1_0 can not be set to more than 150MHz.

If Fvco1_0 is set to one frequency smaller than 150MHz,the output is right.

Please help check the issue,thanks a lot.