This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03318: LMK03318

Part Number: LMK03318

Hello,

  1. I intend to use the STATUS outputs as as LVCMOS33 clock outputs. In this case, the outputs are not Opend drain, am I correct?
  2. How long does it take for the device to load the EEPROM into the device? More importantly, how long does it take from power up until the clock outputs are set?
  3. What is the EEPROM size?

Thank you,

Svetlana.

  • Hello,

    1. Yes, when using STATUS outputs as Single-ended clock outputs, I recommend to configure the status output mode to LVCMOS/push-pull instead of open-drain.

    2. Register initialization from boot EEPROM should be very fast, compared to the overall startup time spec to 10 ms (max, time from POR to Outputs toggling).  Startup time can be 2~4 ms, depending on how you configure the programmable XTAL startup and PLL wait timers.

    3. EEPROM size is 345 bytes.

    Regards,
    Alan