Part Number: LMX2491
Other Parts Discussed in Thread: LMX2492
Hi all.
I would like to get the "Fin Input Sensitivity graph" of LMX2491
I attach the Fin Input Sensitivity of LMX2492.
Is this test condition single-end?
Best Regrads,
Sho
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Noel san
Thank you for your reply.
The characteristics of LMX2491 is the following,
PFin : Power for Fin Pin : Single-Ended Operation : -5dBm@min 、5dBm@max
I am asked the reasen why the minimus PFin is 5db from my customer.
As long as waching to the Figure 4 of LMX2492, Power(dBm) is -10dBm @ 16GHz.
So please tell me the reason about it and test condition in the datasheet.
Is it marginal value?
Best Regards,
Sho
Hi Noel san
I understood what you said, thank you.
I have one more question.
My customer input frequency 750MHz (min -9dB) to Fin,
so I think LMX2492 can receive the above frequency, because Power(dBm) is about -35dBm@750MHz in Figure 4.
Please tell me the comment.
Best Regards,
Sho