Part Number: CDCM9102
Other Parts Discussed in Thread: AM5718,
Tool/software: Linux
Hi,
We have designed single board computer with AM5718. We have PCIe based ethernet peripheral. For PCI we are using CDCM9102 Clock generator. The clock is coming from the crystal. Please see the attached clock input wave form also.
OE is 3.3V
OS0 is 3.3V(pulled up with 100k)
OS1 is 0V (pulled down with 0ohm)
RESET is 3.3V
REGCAP1, REGCAP2 are connected with 10uF 6.3V
VDD1,2,3,4,5,6 Connected with 3.3V
OE Connected with 3.3V
We are not getting the clock on OUT0P, OUT0N and OUT1P, OUT1N. Actually our hardware is production targeted. Because of this it is on hold. Could any one give suggestions.
Thanks & Regards,
Ganesh.T