Part Number: LMX2592
Other Parts Discussed in Thread: LMK61E2, LMK61PD0A2
HI guys,
I am looking to design a LO source using LMX2592 RF synthesizer.
I have few query's regarding LMX2592.
1. What kind of resolution I can expect from LMX2592 between 20MHz to 9.8GHz ?
2. Can I use single output RFout A instead of two outputs ?
3. Does single ouput RFoutA covers all the output frequency range between 20M to 9.8G ?
4. Can I use single ended output instead of differential ?
Can anyone suggest me best 10M to 100M /200M reference clock generator with very low Jitter ?
As of now I am using Onsemi Part which is not very good, it is giving me a Jitter of 15 pico seconds.
Many Thanks,
Satya.