Other Parts Discussed in Thread: LMK04828
Hello,
1) I need to know the typical and max part-to-part skew on this part. This is critical. I'm using 8 parts in parallel and crucially dependent on this parameter.
2) I will be running 8 of these parts in parallel and will be using the SYNC function. If I'm using an output with bypassed selected and use the SYNC pin to synchronize all parts and then when to switch from bypassed to divide-by-2, will I still have synchronization in the divide-by-2? The reason is because I want to use the bypassed mode to check the clock phase, then switch to divide-by-2 and check its phase relative to another parts divide-by-2.
3) If I use "clk en" to turn off a channel, will I lose SYNC from a divide-by-2 mode when I enable the channel again?