This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03318: Frequency Range

Part Number: LMK03318

Dear Team,

Currently we connect crystal(50Mhz) to clk gen’s secref p/n.

According to our crystal measure result, the Frequency tolerance range is over csystal’s spec, and I think we should follow clk gen’s spec.

So we need your help to know clk gen’s Frequency tolerance range. As below picture, which one should we refer to? 25ppm,. 35ppm.or ±50ppm ?

Thanks.

  • Plesse review this app note to understand the pullable crystal specifications that govern the crystal frequency offset (ppm) from nominal frequency by setting the programmable cap load internal to the LMK03318 crystal inputs.

    www.ti.com/.../snaa281a.pdf

    More details of the crystal frequency margining usage & operation can be found in the datasheet applications information section and EVM user's guide.

    Regards,
    Alan