Part Number: LMK04208
LMK04208 devices are programmed using 32-bit registers. How is Microwire connected with SPI of Lanchpad in which 16-bit registers are used?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you.
SPISOMI: SPI slave-output/master-input pin
• SPISIMO: SPI slave-input/master-output pin to DATA
• SPISTE: SPI slave transmit-enable pin to LE
• SPICLK: SPI serial-clock pin to CLK
Is it correct?
Concerning how deal with registers I'll consult MCU forum.