Other Parts Discussed in Thread: CDCV304,
Hi Team,,
My customer design CDCLVP1204 with single end LVCMOS input as below circuit. The INP0 connects with LVCOMS input(from CDCV304) and INNO connects with VAC_REF.
Currently,the VIH=2.3V, VIL=1.3V,so the Vth at INP0 pin is 1.8V,but the Vth at INN0 pin is 2.03V(from VAC_REF).
Is there any issue if the Vth are different in INN0 and INP0?
Best Regards,
Nick Dai