Part Number: CDCV304
The datasheet for the CDCV304 lists a 'continuous total output current' figure in Abs Max table of +/- 50mA.
Does this figure refer to the maximum output current per output pin i.e. total of 200mA across the 4 outputs, or is it the total output current across all 4 pins i.e. 12.5mA output per output pin if loaded equally.
If the later can we run one output continuously at 50mA if the other 3 are not loaded?
Also I assume +/- 50mA means the outputs can sink or source 50mA DC continuous so if we are looking at a clock output we can apply a shape factor / rms value to this?
Thanks