This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03001: Single-ended Sine Wave Input

Part Number: LMK03001

Hello,

My customer has a question about LMK03001.

[Q]

The recommended OSCin power for operation with single-ended sine wave input is shown in Figure 8-14 in the datasheet Page 36.

The frequency range is shown up to 100MHz.

Can it input more than 100MHz ?

May I think about the figures more than 100MHz as follows?

* The slope is -6dB/oct but the bottom is -10dBm for operation with single-ended sine wave input.

Best Regards,

Hiroshi Katsunaga