Part Number: LMK04808
Hi team,
one of my customer meet some problem on LMK04808 configuration:
they want output 6 and output 7 of LMK04808 come from the first stage VCO, and the divider of output 6 and output 7 is 2, but they find the power on configuration will failed some time(the confituration started several seconds after power on), especially in low temperature condition, this will happened every time, but all the other output is right, and both two VCO are locked.
when they configure output 6 and output 7 from the second VCO after power on, and then make a second configuration to change to first VCO, then this failure become much better, but still happens some time.
so do you have some comments on this issue, or do you have some suggestion on configure output 6 and output 7 from the first VCO.
Thanks very much.
Regards, Sunny.