This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK03318EVM: About EVM test condition

Guru 19685 points

Part Number: LMK03318EVM
Other Parts Discussed in Thread: LMK03318

About LMK03318EVM Users manual, is there connection example for LMK03318EVM and Test instruments?

Users manual page-42 is described the name of Test instruments, but connection example is not find.

(Schematic was not described,too)

Best regards,

 Satoshi

  • Hi Satoshi-san,

    Examples of test and measurement setups can be found in the device datasheet. See section 9: 'Parameter Measurement Information' on page 22 of the LMK03318 datasheet. Additionally, sections 10.4.2 'Universal Input Buffer' and 10.4.16 'High-Speed Clock Outputs' show examples of input and output terminations. Finally, section 8 'Device Specifications' lists specific test conditions under which the device specifications were measured.

    Regards,
    -Tim