This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594: Is there an extended temperature range for this IC down to -55C?

Part Number: LMX2594

I have a rather tough requirement to try and meet with respect to temperature, and I was wondering if anyone from TI would be able to help with this. This PLL chip will do exactly what I want it to do, but we need it to operate in an environment down to -55C. Will the LMX2594 or any other PLL that can output a frequency up to 12GHz be able to be operated down to -55C? Thanks.