Part Number: LMK61E2
Other Parts Discussed in Thread: LMK04828
Hello,
I am looking to use the LMK61E2 with the Kintex Ultrascale FPGA from Xilinx for a prototype board and I have a question regarding the LVDS specification. From the LMK61E2 datasheet, the LVDS Output Characteristics of the LMK61E2 seem to be compatible with the FPGA's LVDS specification, but there is a VOUT, DIFF, PP Differential output peak-to-peak swing specification on the LMK61E2 datasheet that confused me. Is the VOUT, DIFF, PP specify the maximum VOH peak-to-peak? Can someone verify that the LMK61E2 is compatible with the FPGA specification below?
Thanks,
-Andrew
FPGA specification:
LMK61E2 specification: