Part Number: LMX2594
Other Parts Discussed in Thread: LMX2492,
The LMX2494 is potentially an excellent alternative to the LMX2492 + external VCO. However, it does not have all of the modulation capabilities present in the LMX2492. My question is: How feasible would it be to modulate the reference input to the PLL as an alternative to using the internal modulation circuitry?
For example, a LFM chirp from say 150 to 200 MHz could be generated with an FPGA + DAC and then passed to the LMX2494 reference input. The LMX2494 would then act as a frequency multiplier. A value of 50 would theoretically result in an output sweep from 7500 MHz to 10,000 MHz. Modulating on the FPGA would provide a great deal more flexibility and perhaps FSK and PSK functionality could be implemented as well. I'm curious to know if TI designers believe there would be any impediments to such a scheme. I would be interested in sweep rates on the order of 5 MHz/us at the RF output or equivalently 0.1 MHz/us at the reference input.
Many Thanks!
David