Other Parts Discussed in Thread: SN74LVC1G125
Hi
I need to supply the 20MHz clock to parraler 25 components, which need this clock.
The components are stacked on top of each other and separated about 1" from each other forming 3 stacks of 8 components 8"long.
I need to distribute the same clock to each of them.
The components have a clock buffer where the clock connects to "SN74LVC1G125".
So the question is: Can I simply connect all of the clock inputs together and run them from a single "SN74LVC1G125" output, or I need to use a specialized clock distribution IC?
How long cables and what type of cable do I need to sitribute the 20MHz clock?
thanks