Part Number: LMK04208
Tool/software: WEBENCH® Design Tools
Hi,
I tried to find a solution for the following clock tree with Webbench:
input: 43.333333 MHz
output 0: 25 MHz
output 1: 25 MHz
output 2: 5 MHz
output 3: 5 MHz
One of the solutions was a design with the LMK04208.
This solution is my preferred one because I need a digital delay for all the outputs, and the other solutions use different parts without digital delays (which took a little time to find out...).
But:
After pressing "Open design" I get a lot of strange results:
1. Webbench suggests a 43.3333 VCXO. This is useless, because such VCXOs are not available
2. Webbench suggests 1191.6667 MHz as VCO frequency. This is outside of the frequency range of the VCO in the LMK04208
3. Dividing 1191.6667 MHz by an integer never leads to 5 MHz or 25 MHz
Summary:
Webbench seems to be useless for designing clock trees.
Is there another tool that works a little better?
Regards
Christian