Part Number: LMX2581EVM
Other Parts Discussed in Thread: CODELOADER, USB2ANY, LMX2581
I have recently purchased an LMX2581 eval board which came with a USB2ANY box; when I try to run this from CodeLoader (version .20.2 on Windows 7) I get a message saying that the USB2ANY firmware needs to be updated. The box serial no. appears to be read correctly so the USB link appears ok. When I disconnect the USB cable and then reconnect whilst pressing the BSL button, the green LED first flashes a few times and then is lit. I then reset the USB2ANY as requested by the next window and hit the OK button. When I then close the Firmware Loader window I get the error messages "u2aOpenError :-6" and then "Failed to open USB2ANY".
I've tried re-starting CodeLoader, rebooting the PC etc. in various combinations but always get the same result. How do I get this to work?