Part Number: DAC3484EVM
Other Parts Discussed in Thread: CDCE62005, DAC3484
I have the DAC3484EVM and TSW1400EVM working together well with the supplied TI Software. Thank you for providing such a great evaluation kit!
I would like to be able to configure the DAC3484 directly (instead of over USB) by connecting to the SPI jumpers for the DAC. However, there is no way to configure the CDCE62005 except over USB.
The CDCE62005 is supposed to (based on my reading of the documentation) store its settings in non-volatile memory and automatically configure itself after a power-up. However, I cannot see this happening.
Whenever I power-up the DAC3484EVM board, I have to toggle the "Wake Up" button in the DAC3484 EVM Software Control GUI a few times before I can see the "LOCK" LED (D1) light up. I suspect the process of toggling the "Wake Up" button is also sending the configuration data down to the CDCE62005.
How can I make the CDCE62005 on the DAC3484EVM automatically wake-up and configure itself from my last used settings?
Thank you!