Part Number: LMK04616
Hello
I'm considering using the device for multi-stage clocking architecture utilizing several of these devices while the last stage will need to drive all 16 outputs independently (and perhaps differently configured frequencies and delays per each output).
From the datasheet I understand that each of these 16 outputs is individually configured for frequency (dividers after PLL2) and delays, i.e. all of 16 outputs are completely independent in configuration from each other.
However the diagrams in the section 9.4 (Figures 51 through 54) suggest that the outputs are boundled in pairs to 8 blocks, i.e. each block drives 2 adjacent differential outputs. The diagrams also suggest that the dividers/delays configuration is idividual for each block (not output), i.e. each two adjacent outputs share the same deviders/delays configuration. Is that correct ? If this is the case, the user cannot have 16 totally inpedentent outputs, but rather 8 independent pairs of differential outputs allowing up to 8 different frequencies and 8 different delay settings
AM I wrong ? Please advise