Part Number: LMX2594EVM
A customer is interested in the LMX2594EVM and have following questions,
1. How easy is it to get up and running with the kit and the software? Can you provide any training?
2. What is the form of the output (Is it a square wave, a sine wave or other)?
3. Can the phase of the output be varied, and if so what is the smallest amount by which it can be adjusted?
4. Can the amplitude of the output be varied, and if so what is the smallest amount by which it can be adjusted?
5. Can the duty cycle of the output be varied, and if so what is the smallest amount by which it can be adjusted?
6. Is a signal strength of 200 mV peak-to-peak (-10dBm) acceptable for the external reference signal?
7. What other requirements on the external reference signal are there?
8. Depopulation of board for single-ended signal?
9. How to use differential pair?
Could anyone help me this please?
Thank you in advance.