Part Number: LMX2594EVM
Other Parts Discussed in Thread: LMX2594
Would someone provide some help regarding the LMX2594 evaluation module questions below:
The board is tuned to 7999MHz, with a 100MHz reference and a 100MHz PFD. The N divider is 79 and the fractional divider is 99/100.
This setup is using the evaluation module direct from the factory.
There are two questions in particular:.
1. Regarding spurious performance of the part. It appears there is an integer boundary spur at 1MHz of about -68dBc. Does that seem accurate? There does not seem to be a spur specification in the EVM documentation or datasheet that seems to correlate.
2. The output power at 7999MHz is about +2dBm. The datasheet says +5dBm is typical. Is that accurate?
Shawn