Dears:
I need help on how to buffer/drive the output of one CDCM61001 source to 9 controllers.
they all use a 75mhz input clock with very low jitter specification.
Can you please recommend a buffer/driver IC.
all the controllers are on SAME pcb and distance to the last one is about 8 inches.
I could rearrange the components to make it 6 inches long.
I could use 2 CDCM61004; but Cost is the issue.
Thank you.
p.s.: the Ti's data sheet says: " A high-quality, low-jiddter differential clock source is required..., LVDS differenctial clock source, Jitter: less than 50 ps pk-pk, Duty cycle: 40 to 60%; rise/fall time: 700 ps.." Thanks