Part Number: LMX2594
In fig 6, Closed Loop PLL at 15G; please clarify what is the frequency range for integrated phase noise = 301.5 mDEg rms?
What is 2nd harmonic content from 15 to 26 GHz? I need a simple test source for BIT (Built IN Test). Greater than -30dBm is fine.
Why not allow connecting the VCO input to divider/phase detector to come from external circuit? This would allow mixing the VCO with a comb line to make a better synth, one with lower N multiplier and better phase noise?
What is PLL speed in tuning? Is a calibration usually needed, and does this slow it down? My goal is < 15usecs to tune to a new frquency after receipt of command on SPI bus.