Other Parts Discussed in Thread: CD74HC297, CD74HC7046A, SN74LS628, LMX2582, LMX2571, LMX2541, LMX2592, LMX2594, LMX2581
I'm looking for a VCO to produce a 12Mhz clock with a tuning range of at least +- 10000PPM . Cost is not a major issue. Simplicity is!
I've looked at
tlc2934(really poor tempco which causes an initial frequency startup issue) and marked as NFND
CD74HC297, CD74HC7046A, CD4046 too low freq at 3.3V
SN74LS628 is 5V, but I like that it has a range input.
I looked at the VCO section of more stable/complex devices with external loop filters and a Vin pin, such as LMX2582, but I'm not sure what would be the best choice once I get that complex. Also, the dynamic tuning range at that frequency isn't obvious. (and how to best convert to a logic level clock).
I guess I can hook up a spi for initial setup, but I can't be doing anything interactive once I start the system.
So, what is the 3.3V (or lower) VCO of choice to generate a logic level clock at 12MHz (or multiples thereof). (low jitter, good tempco, etc)
Thanks
Bruce