Part Number: LMX2594EVM
Other Parts Discussed in Thread: LMX2594
On the LMX2594EVM what tool or formula should I use to determine the L1 pullup inductor in single output mode for 9.4GHz & 9.8GHz?
is it okay to just put a 50-ohm end cap on RFoutAM to enable single mode out on RFoutAP?
Should I remove R38 in single output mode when only using RFoutAP?