Hi,
I require Clock generator with 4 outputs which has different outputs such as (3 number of 200MHz and one 125MHz).
Is there any device which is pre programmed for such outputs or can be programmed through I2C.
Regards,
Nibin Das S
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I require Clock generator with 4 outputs which has different outputs such as (3 number of 200MHz and one 125MHz).
Is there any device which is pre programmed for such outputs or can be programmed through I2C.
Regards,
Nibin Das S
Hi Nibin
Wat are the jitter requirements? CDCE925 can support your requirement. You can also use the WEBENCH® Designer at www.ti.com