This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMX2595EVM: LMX2595 Platinum Software Issue

Part Number: LMX2595EVM
Other Parts Discussed in Thread: LMX2595

Tool/software: WEBENCH® Design Tools

My customer is seeing the following issue with the LMX2595 Platinum Software:

I am currently trying to simulate the LMX2595 PLL w/ integrated VCO in TIs PLLatinum SW.  I have run the simulation to optimize phase noise and everything looks fine.  When I move to the Lock Time Tab, the Frequency Start and Stop values are both 15 GHz.  My settings on the PLL are such that the VCO outputs 8.75GHz and then the output doubler is enabled to get 17.5GHz.  My concern is that the simulation has optimized for phase noise but is perhaps unstable due to what is being shown in the Lock Time tab???  It appears that I can't change the Freq values (they always change back to 15GHz when I try).

Is this normal? Can this variable be changed? Please let me know if this is an issue with the software.

Thanks for your help with this!

Richard Elmquist